Search FAQs
Which ION meter models and firmware supporting IEC61850 communication protocol
Your ION meter must have Ethernet communications and be a model that supports IEC 61850. New meters can be purchased with IEC 61850 or IEC 61850 firmware can be loaded onto an existing meter.
Refer below meter models and meter firmware support IEC 61850:
Meter Model:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008z1IVQAY&oid=00DA0000000abSm)
Meter Firmware:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008z1IQQAY&oid=00DA0000000abSm)
Meter Model:
Meter Firmware:
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: