{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
While using wireless switch XB5 , can we increase the distance from button to receiver 'ZBRRC' using the antennas 'ZBRA1'.
It is possible to increase distance between Harmony XB4/XB5R Transmitter and Receiver unit.
There is no such limitation of the antennas that can installed. But you have to actually know, how much maximum distance will be required between transmitter and receiver unit/units for your application. Also, it is important know ,that whether receiver unit will be freely mounted OR it will be mounted inside the cabinet. Because, if the receiver unit is mounted in a free area, the maximum distance between transmitter and receiver unit will be upto 100m ( No need to install Antenna). If the receiver is mounted in a closed cabinet, you can see that distance reduces to 25m. So, in such situation, you can use install a Relay antenna to increase distance upto 40m and if you want more distance than 40m, you can install another Relay Antenna unit.

Schneider Electric India

While using wireless switch XB5 , can we increase the distance from button to receiver 'ZBRRC' using the antennas 'ZBRA1'.
It is possible to increase distance between Harmony XB4/XB5R Transmitter and Receiver unit. 
There is no such limitation of the antennas that can installed. But you have to actually know, how much maximum distance will be required between transmitter and receiver unit/units for your application. Also, it is important know ,that whether receiver unit will be freely mounted OR it will be mounted inside the cabinet. Because, if the receiver unit is mounted in a free area, the maximum distance between transmitter and receiver unit will be upto 100m ( No need to install Antenna). If the receiver is mounted in a closed cabinet, you can see that distance reduces to 25m. So, in such situation, you can use install a Relay antenna to increase distance upto 40m and if you want more distance than 40m, you can install another Relay Antenna unit. 

Schneider Electric India

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range: