{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does PowerLogic PM5000 series meter has Instrument Transformer correction (ITC) feature. If not, which meter model has ITC this feature.

Instrument Transformer Correction (ITC) allows you to correct for inaccuracies in the current transformers (CTs) and potential transformers (PTs).
The ITC feature is not available with PowerLogic PM5000 series meter's.
ION7550/ION7650 meters are shipped with ITC-capable firmware, its ITC modules (Instr Xformer in the firmware) must be configured using accurate
measurements to ensure valid calculations. There is one Instr Xformer Correction module for each current and voltage input into the meter.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: