undefined [object Object]
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is PRA on Altivar 71 drive.
PRA is Power Removal Function Active (drive locked out).
It is a state of the drive which means that it is locked. If drive displays PRA, that means that you do not have 24 V on the terminal PWR. Normally, all the drive are delivered with a "link" between terminals PWR and +24.
 
This situation is for safety reasons. When the status of ATV71 is PRA, for safety reasons, the software is frozen and nothing is done until PWR and +24 are shunted.
 
The solution is to shunt PWR and +24 before power on the drive.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.