undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Could we use Modbus TCP/IP and IEC61850 protocol with same Connexium Ethernet Switch for using both protocol at the same time.
A managed switch will work on the network connection instead of the specific protocol. So you can use both protocols at a time with our Connexium switches, only you need to take care that the switch that you have selected will be having the management of RSTP for network redundancy.
In  Connexium switch range you can select any of these TCSESM063F2CS1, TCSESM083F23F1, TCSESM063F2CU1 part numbers for this application.

Schneider Electric India

Could we use Modbus TCP/IP and IEC61850 protocol with same Connexium Ethernet Switch for using both protocol at the same time.
A managed switch will work on the network connection instead of the specific protocol. So you can use both protocols at a time with our Connexium switches, only you need to take care that the switch that you have selected will be having the management of RSTP for network redundancy. 
In  Connexium switch range you can select any of these TCSESM063F2CS1, TCSESM083F23F1, TCSESM063F2CU1 part numbers for this application. 

Schneider Electric India

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more