{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the principal working of current transformer supervision protection function in VAMP 255/245/230 relay's.

The device supervise the external wiring between the device terminals and current transformers (CT) and the CT them selves. Furthermore, this is a safety function as well, since an open secondary of a CT, causes dangerous voltages.
The CT supervisor function measures phase currents. If one of the three phase currents drops below Imin< setting, while another phase current is exceeding the Imax> setting, the function will issue an alarm after the operation delay has elapsed.

Schneider Electric India

What is the principal working of current transformer supervision protection function in VAMP 255/245/230 relay's.

The device supervise the external wiring between the device terminals and current transformers (CT) and the CT them selves. Furthermore, this is a safety function as well, since an open secondary of a CT, causes dangerous voltages.
The CT supervisor function measures phase currents. If one of the three phase currents drops below Imin< setting, while another phase current is exceeding the Imax> setting, the function will issue an alarm after the operation delay has elapsed.

Schneider Electric India
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
Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top