{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What are the MTBF values of RXG range electromechanical plug in relays.
As these plug in relay have not electronic part, MTBF data is not relevant.
We can only provide the life time of RXG which depends to the mechanical and electrical durability. For RXG relay, mechanical durability is 10000000 cycle.
Please, refer to the catalog in attachment (see page 4, 5) there are some curves in order to determine the electrical durability of the device following the switching capacity and the use category.
"

Schneider Electric India

Attachment(s)
RXG Catalogue.zip [1.23 MB]