Search FAQs
Will Altistart 01 work when motor is in regeneration mode.
ATS01 will work when motor is in regeneration mode.
If the motor become generator the motor will feed the energy to the network.
When ATS01 is bypassed then the regenerative energy will transferred to the network in steady state condition (like DOL – direct on line starter)
But for deceleration mode, it is not possible to feed the energy into the network. The starter controls the voltage.
If the motor become generator the motor will feed the energy to the network.
When ATS01 is bypassed then the regenerative energy will transferred to the network in steady state condition (like DOL – direct on line starter)
But for deceleration mode, it is not possible to feed the energy into the network. The starter controls the voltage.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: