Search FAQs
How can we read and write bit value of a variable created in Vijeo Designer.
You can use Variable Methods to read extracted bit and write to extracted bit of an Integer variable. The method to read Extracted bit is X and to write to any particular bit XW.
To use this if you have created an integer variable as var_1 then to read bits you can use the following syntax:
var_1.X(0)
This will return bit 0 status of integer variable var_1.
To write to you can use :
VariableName.XW(int position, boolean value);
For example
var_1.XW(0, True);
This will write value true to bit 0 of var_1.
Please take note that write operation can only be performed in Script as its return is INT type.
To use this if you have created an integer variable as var_1 then to read bits you can use the following syntax:
var_1.X(0)
This will return bit 0 status of integer variable var_1.
To write to you can use :
VariableName.XW(int position, boolean value);
For example
var_1.XW(0, True);
This will write value true to bit 0 of var_1.
Please take note that write operation can only be performed in Script as its return is INT type.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: