{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
With Modbus T-junction VW3A8306TF03 or VW3A8306TF10 what is the maximum length of cable that we can use to connect 2 of these modbus T-junction together. Can we increase this length .
This modbus T-junction VW3A8306TF03 or VW3A8306TF10 the maximum length of cable that you can use between two T-Junction box is 10 meters as the ports of this modbus T-junction VW3A8306TF03 or VW3A8306TF10 were isolated ports and this is the limitation of this isolated port.
If you wants to increase the length then he can use two numbers TWDXCAISO (serial link tap isolation box) between the two  modbus T-junction VW3A8306TF03 or VW3A8306TF10 using which this maximum distance can be increased to 1.2 KM.

Schneider Electric India

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.