{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does time and Date of PM5350 meters backed to default after the control power of the meters were lost.

Kindly note that the PM5350's RTC is backed-up by a capacitor (not a battery). So if the clock is set and auxiliary power supply to the meter remains cut-off for more than 30 seconds, next time auxiliary power is restored the RTC will reset to 00:00:00 hrs (date will reset to some value), and start running henceforth. Therefore, in event of Aux. power supply interruption, user must check and set RTC as required.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: