Search FAQs
What is the flame resistance of Acti9 iC60 MCBs.
The raw material used for the case and cover on Acti9 iC60 MCBs comply with glow-wire test at 960 and 650°C according the standard IEC 60695-2-10 and at the fire classification V-2 according the standard UL 94.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: