- Disconnect the entire load connected to UPS.
- Reset the Circuit Breaker present at the back panel of UPS.
- Reconnect the equipment one at a time, if circuit breaker trips again disconnect the device that caused the problem.
- Power on the UPS through Power ON/OFF button.