{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

UPS is giving beep sound and power on/off light flashing for every 6 seconds in UPS BX1000UXI?

Possible Couse: UPS is Over temperature on mains/battery.

The UPS is overheated. Ensure that the operating ambient temperature is within product specifications. Allow a minimum of 20 cm clearance on all four sides of the UPS, for better ventilation.

Note: The UPS will beep and the red LED will illuminate till the internal temperature reaches the normal range.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: