undefined undefined
{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to Set the Overload Outlet Restrictions in AP86** Model ?

Path: Configuration > RPDU > Phase and Bank
Prevent users from applying power to outlets during an overload condition. You can set the following restrictions for each phase and bank:
• None: Users can apply power to outlets regardless of an Overload Alarm or Near Overload Warning.
• On Warning: Users cannot apply power to an outlet on the selected phase or bank if the current for that phase or bank has exceeded the Near Overload Warning threshold.
• On Overload: Users cannot apply power to an outlet on the selected phase or bank if the current for that phase or bank has exceeded the Overload Alarm threshold.


To set Overload Outlet Restrictions:
1. Click the Configuration tab, then RPDU, then Phase or Bank from the menu.
2. Make selections for Overload Outlet Restriction.
3. Click Apply

Schneider Electric India