Search FAQs
What is the meaning of 5P250 - 0.5 in the catalogue for TLPU1 (LPCT)
Thanks to LPCT technology, this type of Current Transformer is able to mix the performances of protection CT and measurement CT, while achieving a linear response all along its current range.
So, 5P250 - 0.5 means :
- 5P250 : 5% tolerance up to 250 times the rated current
- 0.5 : 0.5 class of accuracy for measurement purpose together within the same CT.
So, 5P250 - 0.5 means :
- 5P250 : 5% tolerance up to 250 times the rated current
- 0.5 : 0.5 class of accuracy for measurement purpose together within the same CT.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: