{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to Set the Date and Time in Netbotz 200 ?
Method (Administration>General>Date & Time>mode)
Set the time and date used by the Main Module. You can change the current settings
manually, or through a Network Time Protocol (NTP) Server.
• Manual: Do one of the following:
– Enter the date and time for the Main Module.
– Select Apply Local Computer Time to match the date and time settings of the
computer you are using, and click Apply.
• Synchronize with NTP Server: Have an NTP Server define the date and time for the
Main Module.

Schneider Electric India