{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
I am using CTU_UDINT counter EFB in Unity Pro, but the data in CV overflow above the PV value, why this is happening?
The CTU_**** counter works to the maximum values of the data type being used. No overflow occurs. Since you have used UDINT you should refer to below note about data type UDINT.

UDINT is the abbreviation of Unsigned Double INTeger (encoded in 32 bits). The upper/lower limits are 0 to (2 to the power of 32) - 1. For eg.
0, 4294967295, 2#11111111111111111111111111111111, 8#37777777777, 16#FFFFFFFF.

Schneider Electric India

I am using CTU_UDINT counter EFB in Unity Pro, but the data in CV overflow above the PV value, why this is happening?
The CTU_**** counter works to the maximum values of the data type being used. No overflow occurs. Since you have used UDINT you should refer to below note about data type UDINT.

UDINT is the abbreviation of Unsigned Double INTeger (encoded in 32 bits). The upper/lower limits are 0 to (2 to the power of 32) - 1. For eg. 
0, 4294967295, 2#11111111111111111111111111111111, 8#37777777777, 16#FFFFFFFF.

Schneider Electric India

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top