{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to synchronize the time of HMIGTOXXXX from BMXERT1604

Refer the below step-wise procedure to set the time Sync between HMIGTOXXXX from BMXERT1604T.

1. In the IO Manager section of your Vijeo Designer project, select the Modbus EQUIPMENT that you wish to sync your time from.
2. You will see the Dialog table in the Property Inspector. Select the ellipse to open the Dialog Table Settings window.
3. You will need to check the box in the top left corner to enable the dialog table.
4. Then input a memory word address into the Start Address field. The memory word address should be the address in the Unity processor that is not used in logic.
5. Select the Add button.
6. Scroll to the 33rd function called “Set terminal clock”. Keep in mind that the Set PLC clock takes up 4 words.
7. Change the Time format for the Terminal to BCD.
8. Then select OK

Schneider Electric India

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: