{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to do Port ID numbering in AP5201 ?

Follow the below steps :

Each computer port on an Analog KVM Switch system has a unique assigned Port ID. The Port ID includes two parts: a Station Number and a Port Number.
>  Station NumberóA two-digit number indicating the switch's position in the cascading sequence. The Station Number corresponds to the number displayed on the front panel Station ID LED. The Station
Number precedes the Port Number. ** For the AP5201 8-port KVM, this number will always be 01. ï Port NumberóA two-digit number indicating the corresponding connection port on the switch station.
Station and Port numbers 1 through 9 include a leading zero and display as 01 through 09. For example, a computer attached to Port 6 of Station 12 has a Port ID of 12-06.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: