Search FAQs
What are the characteristics of pulse output of PM2230 energy meter ?
Characteristics of Pulse output (POP) :
Max 40 V DC, 20 mA
20 ms ON time
Configurable pulse weight from 1 to 9999000 (pulse/ k_h)
Max 40 V DC, 20 mA
20 ms ON time
Configurable pulse weight from 1 to 9999000 (pulse/ k_h)
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: