Search FAQs
How RTU Type can be changed in SCADAPack E Configurator and what is the difference between 'Run Wizard' and 'Change RTU Wizard'.
- RTU Type can be changed as View > Change RTU Type
This menu command will run the Change RTU Wizard to allow you to change the currently selected SCADAPack E RTU type, model as well as the WITS DNP3 status and version. The only difference
between the Change RTU Wizard and Run Wizard RTU Type dialog is that you can cancel the action when you run the Change RTU Wizard.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: