Search FAQs
Replace battery indication LED is flickering in UPS BR1000G-IN ?
Possible cause: Battery disconnected , Battery Deep discharged or Battery malfunction.
1. Ensure that the Back-UPS is securely connected to an utility power outlet.
2.Disconnect non-essential equipment from the Back-UPS. Reset the circuit breaker. Re-connect equipment one item at a time. If the circuit breaker is tripped again, disconnect the device that caused the trip.
3. Charge the unit for 6-8 hours .
if above steps fails than The battery is not connected or is nearing the end of its useful life. Replace the battery to rectify the issue.
1. Ensure that the Back-UPS is securely connected to an utility power outlet.
2.Disconnect non-essential equipment from the Back-UPS. Reset the circuit breaker. Re-connect equipment one item at a time. If the circuit breaker is tripped again, disconnect the device that caused the trip.
3. Charge the unit for 6-8 hours .
if above steps fails than The battery is not connected or is nearing the end of its useful life. Replace the battery to rectify the issue.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: