Search FAQs
How to load the previously saved Process Analyst files (.PAV) using a button.
To load the trend file with a button, you can use below function:
ProcessAnalystLoadFile(sPAVFile, iFileLocation, iButtonMask, sObjName )
Define this in the Input field of a button.
As an example, use it as:
ProcessAnalystLoadFile("PA.pav", 0, 1, "AN652")
where 'PA' is the analyst file name which you have already saved from save option in Project Directory.
'0' is the location of file. The default location is "Project folder/Analyst Views".
'1' is the button property (Refer citect help for more button options)
'AN652' is the object name. (double click Process Analyst > Access Tab > check your 'Object Name' under 'identification')
To load this file from other locations from available locations, use 0, 1 or 2. Refer the function help for details.
ProcessAnalystLoadFile(sPAVFile, iFileLocation, iButtonMask, sObjName )
Define this in the Input field of a button.
As an example, use it as:
ProcessAnalystLoadFile("PA.pav", 0, 1, "AN652")
where 'PA' is the analyst file name which you have already saved from save option in Project Directory.
'0' is the location of file. The default location is "Project folder/Analyst Views".
'1' is the button property (Refer citect help for more button options)
'AN652' is the object name. (double click Process Analyst > Access Tab > check your 'Object Name' under 'identification')
To load this file from other locations from available locations, use 0, 1 or 2. Refer the function help for details.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: