Search FAQs
What are the mounting options available for Compact NSXm circuit breakers.
Compact NSXm may be mounted vertically, horizontally or flat on their back or on their side without any derating of characteristics.
These devices can be mounted on a DIN rail using the integrated DIN rail mounting feature.
For backplate mounting, the devices are supplied with two mounting screws (M4),washers and nuts.
These mounting screws can be inserted through mounting holes molded into the device case and threaded into the mounting enclosure, rails or plate.
These devices can be mounted on a DIN rail using the integrated DIN rail mounting feature.
For backplate mounting, the devices are supplied with two mounting screws (M4),washers and nuts.
These mounting screws can be inserted through mounting holes molded into the device case and threaded into the mounting enclosure, rails or plate.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: