Search FAQs
Not able to access the user interface (UI) of NMC card AP9635?
Probable Cause & Solution:
•Verify that HTTP or HTTPS access is enabled.
• Make sure you are specifying the correct URL — one that is consistent with the security system used by the NMC. SSL requires https, not http, at
the beginning of the URL.
• Verify that you can ping the NMC.
• Verify that you are using a Web browser supported for the NMC.
• If the NMC has just restarted and SSL security is being set up, the NMC may be generating a server certificate. The NMC can take up to one minute
to create this certificate, and the SSL server is not available during that time.
Released for:Schneider Electric India
Explore more
Product:
Explore more
Product: