Search FAQs
In UPS BX1100C-IN, Mains is available but still ups is running on Battery mode ?
Probable cause:
It can be because of anyone reason listed below :
It can be because of anyone reason listed below :
- Input socket issue
- Distorted input voltage
- Line voltage out of range.
- Verify that the power cable plug is securely connected to the wall outlet, There should not be any loose connection.
- Verify that the wall outlet is receiving utility power by checking it with another device like mobile charger.
- Input voltage should be between 145V-290V and frequency 50Hz.
- Earth voltage shouldn't exceed 5v and Neutral line must be present without any break.
- If the input supply is coming from generator, check the generator settings and capacity
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: