Search FAQs
Video: How to disable Battery Saver mode for BX600C-IN ?
To disable battery saver option,kindly follow the below steps :
* Press the BATTERY SAVER button to deactivate the battery saver feature.
* Battery saver LED will turn off indicating that the battery saver mode is disabled .
Note: If the load is less than 40 watts we would sugget to disable battery saver mode.We recommend the battery saver mode to be enabled if the load is more than 40 watts for the enchancement of battery life.
* Press the BATTERY SAVER button to deactivate the battery saver feature.
* Battery saver LED will turn off indicating that the battery saver mode is disabled .
Note: If the load is less than 40 watts we would sugget to disable battery saver mode.We recommend the battery saver mode to be enabled if the load is more than 40 watts for the enchancement of battery life.
Released for:Schneider Electric India
Explore more
Product:
Explore more
Product: