To disable the battery-saver option, kindly follow the below steps :
* Press the BATTERY SAVER button to deactivate the battery saver feature.
* Battery saver LED will turn off indicating that the battery saver mode is disabled.
Note: If the load is less than 40 watts we would suggest disabling battery-saver mode. We recommend the battery saver mode to be enabled if the load is more than 40 watts for the enhancement of battery life.
Released for:Schneider Electric India