Which IP Rating enclosure should be used for contactor in high chemical environment.
When contactor are used in chemical environment we strongly recommend using IP6X protection enclosure or minimum IP5X with pressurization system to avoid chemical vapor to get inside enclosure.
Released for:Schneider Electric India
Explore more
Range:
AVEVA™ Plant SCADA
TeSys Control Relays
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.