{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Is The polarity of terminal A1 and A2 from contactor Tesys Green is A1(+) and A2(-) or can customer connect any polarity in the A1 and A2.
On TeSys D with coil AC/DC (LCxDxxBNE or LCxDxxEHE or LCxDxxKUE or LCxDxxUSE), no need to respect polarity when controlled in DC. The poles  A1 and A2 are noted without sign + or -.
On TeSys D with coil DC only (LCxDBBE), the polarity shall be respected. The poles are noted A1+  and A2-.  In case the connections are reversed, the contactor won't close. However, this misconnection won't destroy the contactor. Correcting the wiring will fix the trouble.

 

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top