Search FAQs
Which parameters are available in EM1000,EM1200 and EM1220 meter?
The following parameters are available in EM1000/EM1200 meter :-
PF PF1 PF2 PF3 Power Factor
W W1 W2 W3 / Active Power
VA VA1 VA2 VA3 / Volt-amperes
VAR VAR1 VAR2 VAR3 Volt-amperes reactive
KWh / KVAh / KVARh Watt-hours / Volt-ampere hours / Volt-ampere reactive hours
Run.h Running Hours
On.h On hours
INTR Number of power interruptions
PF PF1 PF2 PF3 Power Factor
W W1 W2 W3 / Active Power
VA VA1 VA2 VA3 / Volt-amperes
VAR VAR1 VAR2 VAR3 Volt-amperes reactive
KWh / KVAh / KVARh Watt-hours / Volt-ampere hours / Volt-ampere reactive hours
Run.h Running Hours
On.h On hours
INTR Number of power interruptions
Released for:Schneider Electric India
Attachment(s)
Explore more
Range:
Explore more
Range: