{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Do MiCOM P24x relays conforms to Power Frequency Magnetic Field Immunity tests.

The MiCOM P24x relays conforms to Power Frequency Magnetic Field Immunity tests as per EN / IEC 61000-4-8, Level 5,
100 A/m applied continuously, 1000 A/m applied for 3 s.
-> As for EN / IEC 61000-4-9, Level 5,
1000 A/m applied in all planes.
-> As for EN / IEC 61000-4-10, Level 5,
100 A/m applied in all planes at 100 kHz and 1 MHz with a burst duration of 2 s.

Schneider Electric India