{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the memory types of Sepam 10 & 20 Range.

Sepam 10:
Sepam 10N and Sepam 10B don’t use any batteries. Only Sepam 10A owns a battery (1/2 AA 3.6 V lithium battery) used to back up the internal clock.
But the events are save in EEPROM and they aren't lost in case power off or reboot.

Sepam 20:
Sepam 20 doesn’t use any battery. Sepam settings are saved in Eeprom memory and disturbance recording data are not saved in case of Power off occurrence.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: