SmartStruxure Server Device Reset Functions
Type | Triggered by | Description | Variable values | Configuration, Historic database | IP settings |
Warm start | Command from WorkStation | Stops the SmartStruxure server device application and then restarts the application. | Affected according to the configured retain levels for the variables | Retained | Retained |
Cold start | Command from WorkStation | Stops the SmartStruxure server device application and then restarts the application. | Affected according to the configured retain levels for the variables | Retained | Retained |
Reset | Short push on Reset button Power return | Stops the SmartStruxure server device application and the operating system and then restarts the operating system and the application. | Affected according to the configured retain levels for the variables | Retained | Retained |
Reset to DFU mode | 3 pushes on Reset button within 2 seconds | Puts the SmartStruxure server device into DFU mode, which enables Device Administrator to communicate with the server. | Not applicable | Not retained | Not retained |
Parameters and variables that are used to define the system or contain important data in the SmartStruxure server device can be retained in a permanent memory. These parameters and variables are automatically saved in the event of power failure, or request for restart and are reloaded after startup.
You can define what kind of events that retention for the parameters and variables should apply.