AS-P and AS-B are delivered without any software. Below is the procedure to install the software.
-
Start Device Administrator.
-
Connect a USB 2.0 cable (maximum length 3 m) to the USB device port on the SmartStruxure server device and a USB port on the PC:
- For Automation Server, use a USB type-A male to type-B male cable.
- For AS-P and AS-B, use a USB type-A male to mini-B male cable. - In the Connection column for the SmartStruxure server device, ensure that usb is displayed.
- Select AS-P or AS-B in the list.
- Click Upgrade device(s)
- In the Upgrade Device box, click New Database.
- Click OK.
Released for:Schneider Electric India