AS-B has two types of memory:
- 256 MB DDR2 SDRAM (for program execution)
- 4 GB eMMC memory (for storage)
If a power failure occurs, all important variables are automatically saved to the eMMC memory before complete shutdown. When power returns, this data retention function ensures that AS-B can continue to run with the correct set of values.