{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Which materials are used for ACTI9 MCB Terminal Plating?

Incoming Terminal from 0.5 Amp to 25 Amp material used is Steel and is coated with Tin.
Incoming Terminal from 32  Amp to 63 Amp Material used is Copper and is coated with Tin.
Outgoing Terminal from 0.5 Amp to 25 Amp material used is Steel and is coated with Tin.
Outgoing Terminal from 32  Amp to 63 Amp Material used is Copper and is coated with Silver.
Terminal Clamp from 0.5 Amp to 63 Amp Material used is Ferrous Alloy and coated with zinc

Schneider Electric India

Attachment(s)

Acti9 terminal details.PNG.pngActi9 terminal details.PNG.png [48.56 KB]