{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the specifications of DigitalInputs in WIMO6CP10

The unit can collect status information and alarm signals via 3 digital inputs (terminals X2B: 3-5). The three digital inputs in
WIMO use an internal 12 V dc auxiliary voltage of the unit (terminal X2B: 8).
Potential-free contacts must be available in the protected object for transferring status information to the unit.
Refer the attached snapshot.

Schneider Electric India

Attachment(s)

WIMO6CP10_DigitalInputs.JPG.jpgWIMO6CP10_DigitalInputs.JPG.jpg [28.02 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: