{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to create a Filtered Alarm View to view the desired alarms only in EcoStruxure Building Operation.

You create an Alarm View to apply an alarm filter that displays only those alarms the user needs to see. Below is the procedure.

1. In WorkStation, in the System Tree pane, ​select the folder or EcoStruxure BMS server where you want to create the Alarm View.
2. On the File menu, point to New and then click View .
3. In the Create Object wizard, in the object type list, click Alarm View .
4. In the Name box, type a name for the Alarm View.
5. In the Description box, type a description for the Alarm View and click Create .
6. In the System Tree pane, select the Alarm View you created.
7. On the Actions menu, click Edit standard Alarm View filter to filter the Alarm View.
8. In the Select Conditions dialog box, click the Add condition button   and select a condition type.
9. Type the condition for the filter.
10. Click the Add row button   to add another condition of the same type.
11. Type the condition for the filter and click OK.

Schneider Electric India

Explore more
Range:
RNG ConduitsTDC Cabling & fixingEcoStruxure™ Building Operation
Explore more
Range:
RNG ConduitsTDC Cabling & fixingEcoStruxure™ Building Operation
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.