Search FAQs
What are Action Notes and what is the use of them inside EcoStruxure Building Operation.
Action notes are grouped by category, with possible actions that may correct the problem listed in each category. An action note specifies the actions that you used to correct the problem that caused the alarm.
Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.
Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics
Reporting the actions that were taken is either voluntary or mandatory. You can configure the alarm so the user is required to report the actions when certain events occur, such as when an alarm is disabled.
Action notes can be of great use the next time the same alarm is triggered or when extracting alarm statistics
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: