Search FAQs
Basic programming of ATV310
Below are parameters if start command and frequency are given from terminals (i.e cmd via pushbutton & speed via potentiometer) of the drive.
Below are parameter need to be set according to the details given in motor nameplate.
301 Standard Motor Frequency
302 Rated Motor Power
304 Rated Motor Voltage
305 Rated Motor Current
306 Rated Motor Frequency
307 Rated Motor Speed
307 Rated Motor Speed
Parameter Value
401 Reference channel 1 = 01
404 Reverse Inhibition = 00
406 Channel Configuration = 01
502.0 Acceleration = 03 sec Put the value as per application in seconds.
501.1 Deceleration = 03 sec Put the value as per application in seconds.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: