Search FAQs
How many profibus devices can be connected with TCSEGPA23F14 PRM module in one segment.
Profibus devices are connected in a bus structure. Up to 32 stations (master or slaves) can be connected in one segment. The bus is terminated by an active bus terminator at the beginning and end of each segment. Both bus terminations must always be powered. When more than 32 stations are used, repeaters (line amplifiers) must be used to connect the individual bus segments.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: