{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to change the password in vamp relays.
Changing the password is possible using VAMPSET or any PC terminal program and
the command line interface of the device.
Example: Changing the configurator password from 2 to 1234 with VAMPSET.
1. Start VAMPSET and connect to the device
2. Open the configurator password either by typing “2” in “Device Setup” window, or
select “Configurator” and type “2” in “Select Access Level” window
3. Select “DEVICE INFO” from the left menu
4. Write “1234” to “Change password” parameter. VAMPSET will ask for confirmation
of the new password

Schneider Electric India