{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
How to reset password , if you forget the password: Vamp relays
if you forget the password(s), it is possible to set them back to default.
Start VAMPSET and select menu "Communication"/"Terminal"
Try to open CONFIGURATOR access level:
> set pwd=2
!! Error Wrong password!
The password has been changed from the factory default 2. After trying three times with
an incorrect password, the password opening will be locked for 20 minutes.
Let's break the passwords:
> get pwd_break
6293293
This number is needed for the breaking. Also the serial number is needed:
> get SerNo
1201

Note: Please, do keep the auxiliary power on until the end of this break-procedure.

Contact VAMP Ltd: vampsupport@vamp.fi or concerned CCC and attach the pwd break number '6293293'
and the serial number '1201'. We will give you a device specific break code which returns
the passwords back to default.

> set pwd_break=4917022. Break the passwords. The '4917022' is the break code you
got from VAMP Ltd. Now the passwords are back to default; 1 and 2.
> set pwd=2. Try to open the CONFIGURATOR access level with the default password
> OK
> set Change_pwd=284593276. Change the CONFIGURATOR password again (This
value is sure easy to forget!).
> set pwd=1 Change also the OPERATOR password.
> set Change_pwd=1845932765

Schneider Electric India