Search FAQs
How to update firmware in MP Series controllers.
Below is the procedure to update firmware in MP Series Controllers:
- In WorkStation, in the System Tree pane, click Server .
- In the List View, click Control Panel .
- In Control Panel, under BACnet , click MP-X Devices .
- When the simple Search pane displays, select the MP Series controller(s).
- In the Actions menu, point to Device , point to Upgrade firmware and then click Select device firmware .
- In the Select Firmware box, click Browse and then select an MP Series controller firmware file to upload.
- Click Download firmware to download the firmware to the MP Series controller(s).
- Select the preferred Activation method: Manually , Immediately , or at a specified Time and Click OK .
- In the simple Search pane, check the Upgrade progress column to view and monitor update status.
- Right-click on the column heading bar and click Add/Remove columns.
- In the Add/Remove columns dialog box, select Application software version to view the currently installed software and Click OK .
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: