Yes, it can handle simultaneouse requests for both Implicit & Explicit exchange. However, the number of requests to be processed per cycle should taken care from all communication ports. This means that requests from other clients like communication EFs, IO Scanner, connected HMI and so on should also be taken into account. No. of request vary from processor to processor.