{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Programming switch weight factors in VAM 3L and VAM 3LX, VAM 10L / VAM 10LD, VAM 12L / VAM 12LD only

The programming switches have different weight factors. To create
an address for the I/O unit, turn switches with different values to the
ON position and calculate the sum of their weight factors. The
following table shows the weight factors of each programming switch

Refer the table attached.

Schneider Electric India

Attachment(s)

weight factor.JPG.jpgweight factor.JPG.jpg [31.05 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: