{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the use of Programming switches for VAM 12L / VAM 12LD
When the L>ext/int DIP switch is in “L>int” position, the output relays
are only activated by dedicated sensors.
SENSOR 1 activates T1.
SENSOR 2 activates T2.
SENSOR 3 activates T3.
SENSORS 4 to 10 are normally sending light information to system
according to zone setting.
If the switch is in “L>ext” position, all output relays are also controlled
by the selected zone information. This activation source can be any
sensor channel 4 to 10 or from an external I/O unit configured to the
same zone.

Schneider Electric India

What is the use of Programming switches for VAM 12L / VAM 12LD
When the L>ext/int DIP switch is in “L>int” position, the output relays
are only activated by dedicated sensors.
SENSOR 1 activates T1.
SENSOR 2 activates T2.
SENSOR 3 activates T3.
SENSORS 4 to 10 are normally sending light information to system
according to zone setting.
If the switch is in “L>ext” position, all output relays are also controlled
by the selected zone information. This activation source can be any
sensor channel 4 to 10 or from an external I/O unit configured to the
same zone.

Schneider Electric India
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
move-arrow-top