Search FAQs
How can I update a BM• CRA 312 •0 (e)X80 EIO adapter module that is not yet configured?
BM• CRA 312 •0 module receives its IP address from the CPU at startup. If the CPU is not configured or the firmware version of the BM• CRA 312 •0 module is not compatible, the BM• CRA 312 •0 module does not receive an IP address.
Set the rotary switches on the BM• CRA 312 •0 module to stored. Power cycle the BM• CRA 312 •0 module. Connect the BM• CRA 312 •0 module via its service port to Unity Loader using the IP address: 10.10.mac5.mac6.
Set the rotary switches on the BM• CRA 312 •0 module to stored. Power cycle the BM• CRA 312 •0 module. Connect the BM• CRA 312 •0 module via its service port to Unity Loader using the IP address: 10.10.mac5.mac6.
Released for:Schneider Electric India
Explore more
Range:
Explore more
Range: